CONFIG_LOGBUFFER in u-boot 2014

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CONFIG_LOGBUFFER in u-boot 2014

1,319 Views
shubhasingh
Contributor I

Hi,

I want to enable logbuffer in u-boot for post result information access in kernel. When i had enabled CONFIG_LOGBUFFER in u-boot for P1020 RDB board,

its stucking after

"

Flash:  16 MiB

L2:    256 KiB already enabled

NAND:  32 MiB

MMC:   FSL_SDHC: 0

*** Warning - bad CRC, using default environment

In:    serial

Out:   logbuff

Err:   logbuff"

Can some body give some pointer where should i look for resolving this.

Regards,

Shubha

0 Kudos
Reply
1 Reply

1,129 Views
alexander_yakov
NXP Employee
NXP Employee

Please look this link at U-boot vendor site:

WarningBadCRCUsingDefaultEnvironment < DULG < DENX

0 Kudos
Reply