Booting fail with CONFIG_PROFILE_ALL_BRANCHES

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Booting fail with CONFIG_PROFILE_ALL_BRANCHES

1,863 次查看
arnobghosh
Contributor I

I am trying to booting profile all branches kernel in ep8248e board which has Freescale MPC8248 processor.

Kernel booting is failing when CONFIG_PROFILE_ALL_BRANCHES is enabled in MPC8241 processor.

It gets stuck after Finalizing device tree ....

Memory <- <0x0 0x8000000> (128MB)

zImage starting: loaded at 0x00900000 (sp: 0xf0001d20)
Allocating 0x8d2838 bytes for kernel ...
gunzipping (0x00000000 <- 0x0090e000:0x00ca6378)...done 0x880dc0 bytes

Linux/PowerPC load:
Finalizing device tree... flat tree at 0xcb3300

0 项奖励
回复
3 回复数

1,473 次查看
alexander_yakov
NXP Employee
NXP Employee

Please specify which Linux BSP you are using, and where it was obtained from?


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,473 次查看
arnobghosh
Contributor I

Linux BSP is build from git://git.freescale.com/ppc/sdk/linux.git

Git tag checkout : fsl-sdk-v1.4

0 项奖励
回复

1,473 次查看
alexander_yakov
NXP Employee
NXP Employee

I do not see MPC8248 processor listed as supported in SDK 1.4

0 项奖励
回复