AP Core TLB not ready on boot (P2020)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AP Core TLB not ready on boot (P2020)

ソリューションへジャンプ
1,930件の閲覧回数
alexy_torres-au
Contributor I

Hello,

I am writing a bootloader (I cannot use U-Boot in my project) that starts the Core 1 of the P2020 as follows:

1. Copy the Core 1 boot core to 0x00800000 (with branch at 0x00800FFC).

2. Set the BPTR at 0x00800000 (and enable page translation)

3. Release the Core1

However, I see while debuging that the Core1 boots correctly to 0x00800FFC, but the TLB is not correct. Indeed it still translates to 0xFFFFF000 -> 0xFFFFF000 for the entry 0.

So Core 1 crashes. 

When I update the TLB by hand thanks to the debuger and set the entry 0 to translate: 0x00800000 -> 0x00800000 it works and the Core 1 is able to boot and works perfectly!

I am sure I am missing something during the initialization but cannot find it. Do you have any idea on how to debug this?

Thanks

タグ(5)
0 件の賞賛
1 解決策
1,727件の閲覧回数
ufedor
NXP Employee
NXP Employee

ba 0x800000

This is your problem.

You have to use relative addressing - not absolute.

元の投稿で解決策を見る

0 件の賞賛
10 返答(返信)
1,727件の閲覧回数
ufedor
NXP Employee
NXP Employee

2. Set the BPTR at 0x00800000 (and enable page translation)

Please consider that in the P2020 QorIQ Integrated Processor Reference Manual, 4.4.4 Boot page translation register (Reset_BPTR) it is written:

"8–31
BOOT_PAGE
Translation for boot page. If enabled, the high order 24 bits of accesses to 0x0_FFFF_Fnnn are replaced with this value."

BPTR.jpg

For the address 0x0_00800000 it is needed to set BPTR=0x80000800

0 件の賞賛
1,727件の閲覧回数
alexy_torres-au
Contributor I

Yes sorry I should have been more precise. I set the BPTR to point to 0x00800000 so I set it to BPTR=0x80000800.

According to what you wrote this is already how I set it. Sorry for the confusion and thank you for the precision.

0 件の賞賛
1,727件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please confirm that you have configured LAW for the address 0x00800000.

0 件の賞賛
1,727件の閲覧回数
alexy_torres-au
Contributor I

I configured a LAW of 1gb starting at 0x0000_0000. Core 0 correctly runs with this configuration and core 1 too if I set the tlb manually before the first fetch.

0 件の賞賛
1,727件の閲覧回数
ufedor
NXP Employee
NXP Employee

You wrote:

 Indeed it still translates to 0xFFFFF000 -> 0xFFFFF000 for the entry 0.

And this is correct - refer to the P2020 QorIQ Integrated Processor Reference Manual, 4.3.3 Boot page translation.

BPTR (if enabled) works with real/physical address after MMU translation is performed.

Please provide screenshot of a debugger window showing assembler code starting from address 0x00800FE0.

0 件の賞賛
1,727件の閲覧回数
alexy_torres-au
Contributor I

Here is the screenshot, you can also find information about the LAW in the upper right corner.Screenshot from 2020-02-21 20-57-03.png

0 件の賞賛
1,727件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please provide screenshot for the code at physical address 0x00800FFC.

0 件の賞賛
1,727件の閲覧回数
alexy_torres-au
Contributor I

Sorry I didnt see the address on the screenshot was 0xFFFFFFFC

Here is a screenshot at 0x00800FFC (physical):
Screenshot from 2020-02-24 12-14-19.png

Here is the code used to enable core 1:

volatile unsigned int* bptr_reg;

printf("Booting CPU1 \n\r");

/* Change the BPTR value to point to 0x800000 (boot page) */
bptr_reg = (unsigned int*)(CCSBAR_BPTR_OFFSET + CCSBAR_BASE_ADDR);
*bptr_reg = 0x80000800;

copy_boot();

/* Kickstart the CPU 1 */
asm volatile (
"isync\n\t"
"msync\n\t"
"isync\n\t"
"lis 4, 0xE000\n\t"
"lis 3, 0x0200\n\t"
"lwz 5, 0x1010(4)\n\t"
"or 3, 3, 5\n\t"
"stw 3, 0x1010(4)\n\t"
:
:
:
);

copy_boot just copies the boot code to the boot page.

Here is the boot code for Core 1:

__ap_start:

# Enable MCHK and debug
lis r3, 0x0200
ori r3, r3, 0x1200
mtmsr r3

# Manage L1 Caches
li r3, 0x2
mtspr 0x3F2,r3 /* invalidate d-cache */
mtspr 0x3F3,r3 /* invalidate i-cache */

# Map Kernel
create_tlb1_entry 1, 9, 1, 0, 0, BOOKE_PAGESZ_16M, 0, \
MAS2_G, 0, MAS3_SW | MAS3_SR | MAS3_SX | MAS3_UW | MAS3_UX | MAS3_UR);

# Set stack
lis r3, 0xFF
mr r1, r3

# Jump to init AP C function.
loop_inf:
b loop_inf

__ap_start_end:

# Rest of the boot page until 0xFFC is padded with 0

__ap_reset:
ba 0x800000

But the code seems to crash when fetching the first instruction.

0 件の賞賛
1,728件の閲覧回数
ufedor
NXP Employee
NXP Employee

ba 0x800000

This is your problem.

You have to use relative addressing - not absolute.

0 件の賞賛
1,727件の閲覧回数
alexy_torres-au
Contributor I

Definitely my problem. It works with a relative branch.

I didn't understand correctly the role of the BPTR and did not understand that the translation was done after the CPU, I thought it was a register the CPU was loading at reset and setting its TLB accordingly.

Thanks for the clarification!

0 件の賞賛