83xx power consumption & Temperature

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

83xx power consumption & Temperature

1,227件の閲覧回数
johndo
Contributor I

I have an MPC8313 133MHz with FLASH, DDR2 & Ethernet. Power Consumption goes up with temperature by 30% or more as it warms up. Does 8313 power go up with temperature?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,054件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Yes, device power consumption raises with junction temperature.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,054件の閲覧回数
johndo
Contributor I

Does NXP/FS have a spreadsheet tool or anything to help calculate power? Datasheet has limited info. I am seeing a 1W increase just by ambient warming up.

0 件の賞賛
返信