nxq1txh5 , coil connection / pinning

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

nxq1txh5 , coil connection / pinning

Jump to solution
1,338 Views
ysellin
Contributor II

Hello,

 

in NXP eval board and datasheet i see that the coil is connected to pins 23+24 on one side and the other side goes through the capacitors to pins 17+18.  The diode being connected to the middle point (between coil and capas).

 

What happens if we invert:

I.e. coil connected to 17+18 then goes through the capacitors to pins 23+24.  The diode being still connected to the middle.

Any problem to expect ?

Thanks for your help.

0 Kudos
Reply
1 Solution
1,330 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

 

No problem is expected if you connect the capacitors of the LC tank on pins 23+24 instead of 17+18 with the configuration you mentioned in your question. Both OUT1 and OUT2 are the same, so, you should not have any problem with this configuration.

 

Regards.

Jose

View solution in original post

1 Reply
1,331 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

 

No problem is expected if you connect the capacitors of the LC tank on pins 23+24 instead of 17+18 with the configuration you mentioned in your question. Both OUT1 and OUT2 are the same, so, you should not have any problem with this configuration.

 

Regards.

Jose