Hello,
in NXP eval board and datasheet i see that the coil is connected to pins 23+24 on one side and the other side goes through the capacitors to pins 17+18. The diode being connected to the middle point (between coil and capas).
What happens if we invert:
I.e. coil connected to 17+18 then goes through the capacitors to pins 23+24. The diode being still connected to the middle.
Any problem to expect ?
Thanks for your help.
Solved! Go to Solution.
Hi,
No problem is expected if you connect the capacitors of the LC tank on pins 23+24 instead of 17+18 with the configuration you mentioned in your question. Both OUT1 and OUT2 are the same, so, you should not have any problem with this configuration.
Regards.
Jose
Hi,
No problem is expected if you connect the capacitors of the LC tank on pins 23+24 instead of 17+18 with the configuration you mentioned in your question. Both OUT1 and OUT2 are the same, so, you should not have any problem with this configuration.
Regards.
Jose