nxq1txh5 , coil connection / pinning

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

nxq1txh5 , coil connection / pinning

跳至解决方案
1,460 次查看
ysellin
Contributor II

Hello,

 

in NXP eval board and datasheet i see that the coil is connected to pins 23+24 on one side and the other side goes through the capacitors to pins 17+18.  The diode being connected to the middle point (between coil and capas).

 

What happens if we invert:

I.e. coil connected to 17+18 then goes through the capacitors to pins 23+24.  The diode being still connected to the middle.

Any problem to expect ?

Thanks for your help.

0 项奖励
回复
1 解答
1,452 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi,

 

No problem is expected if you connect the capacitors of the LC tank on pins 23+24 instead of 17+18 with the configuration you mentioned in your question. Both OUT1 and OUT2 are the same, so, you should not have any problem with this configuration.

 

Regards.

Jose

在原帖中查看解决方案

1 回复
1,453 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi,

 

No problem is expected if you connect the capacitors of the LC tank on pins 23+24 instead of 17+18 with the configuration you mentioned in your question. Both OUT1 and OUT2 are the same, so, you should not have any problem with this configuration.

 

Regards.

Jose