nxq1txh5 , coil connection / pinning

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

nxq1txh5 , coil connection / pinning

ソリューションへジャンプ
1,449件の閲覧回数
ysellin
Contributor II

Hello,

 

in NXP eval board and datasheet i see that the coil is connected to pins 23+24 on one side and the other side goes through the capacitors to pins 17+18.  The diode being connected to the middle point (between coil and capas).

 

What happens if we invert:

I.e. coil connected to 17+18 then goes through the capacitors to pins 23+24.  The diode being still connected to the middle.

Any problem to expect ?

Thanks for your help.

0 件の賞賛
返信
1 解決策
1,441件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi,

 

No problem is expected if you connect the capacitors of the LC tank on pins 23+24 instead of 17+18 with the configuration you mentioned in your question. Both OUT1 and OUT2 are the same, so, you should not have any problem with this configuration.

 

Regards.

Jose

元の投稿で解決策を見る

1 返信
1,442件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi,

 

No problem is expected if you connect the capacitors of the LC tank on pins 23+24 instead of 17+18 with the configuration you mentioned in your question. Both OUT1 and OUT2 are the same, so, you should not have any problem with this configuration.

 

Regards.

Jose