how to connect 6 battery cells

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to connect 6 battery cells

4,335 Views
suvasis
Contributor I

hi

I recently purchased,  RDDRONE-BMS772, can anyone confirm the battery connections are good in the image nelow:

image (1) (1).png

 

0 Kudos
Reply
6 Replies

4,209 Views
suvasis
Contributor I

Can anyone pls reply? I am stuck..

0 Kudos
Reply

4,324 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi 

please refer to the Figure 13. in the UM11421 attached. Please also refer to the following notes.

JozefKozon_8-1685520343478.png

Please refer to the section 3.2 in an UM11421 attached. You need to connect a battery pack to JP1 connector with minimally 3, maximally 6 Cells. To use the Cells is mandatory. Easiest is to connect battery pack with 6 Cells. 

 

JozefKozon_4-1685519683313.png

And you need to set the jumpers along the number of Cell you have connected. Please refer to the page 3. in the schematic attached. 

 

JozefKozon_5-1685519767292.png

The individual Cell voltage must be within the voltage range stated in the Table (-0.3V to 5V) in the MC33772B product page.

JozefKozon_6-1685519815141.png

The Supply voltage is stated from 6V to 30V, but for the RDDRONE-BMS772 the maximum supply voltage is lower. Only 26V. So please follow the UM11421 definition to be safe. 

 

JozefKozon_7-1685519842174.png

 

 

0 Kudos
Reply

4,298 Views
suvasis
Contributor I

hi

In a 4 cell configuration the bms reading for the 4th cell is 0 and other 3 cells are correctScreen Shot 2023-06-02 at 1.35.54 PM.pngScreen Shot 2023-06-02 at 1.36.37 PM.png. Images are attached:

Pls let me know what needs to be checked. 

0 Kudos
Reply

4,296 Views
suvasis
Contributor I

here are the configurations imagesScreen Shot 2023-06-02 at 1.36.16 PM.pngScreen Shot 2023-06-02 at 1.36.22 PM.pngScreen Shot 2023-06-02 at 1.36.28 PM.png

0 Kudos
Reply

4,295 Views
suvasis
Contributor I

hi,

Here are images of the Screen Shot 2023-06-02 at 1.35.28 PM.pngScreen Shot 2023-06-02 at 1.35.41 PM.pngScreen Shot 2023-06-02 at 1.35.48 PM.pngreadings from cell 1, 2, and 3,

 

0 Kudos
Reply

4,135 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Suvasis,

I have checked your connection and it is correct. 

JozefKozon_0-1686041599128.png

Please measure the Cell #4 voltage with the multimeter on the JP1 connector? The VBATT voltage shows 15.5V, which is approximately 4*3.9V. Perhaps the cable on the Cell #4 is damaged. 

With Best Regards,

Jozef

0 Kudos
Reply