frdm-pf1550evm and frdm_KL25Z

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

frdm-pf1550evm and frdm_KL25Z

2,336 Views
HeMyFAE
NXP Employee
NXP Employee

Dear PMIC support,

Our customer download the SW package to support the PF1550 and it came only with the GUI.

Our customer is looking for the actual KL25 i2c driver application code that is required to work in combination with the GUI running on the PC to program the PMIC.

https://www.nxp.com/support/developer-resources/evaluation-and-development-boards/analog-toolbox/pf1...

Regards,

hy

Labels (1)
0 Kudos
Reply
2 Replies

2,205 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Hy,

We do not provide full source code, but I will send you internally a corresponding binary file for the KL25Z MCU. 

I hope it helps.

Best regards,

Tomas

0 Kudos
Reply

2,084 Views
Jerry_H
Contributor I

Hi Tomas,

 

we are having the same problem.
Do you provide the full source code now or is it possible that you send me the binary file too?

Kind regrads

0 Kudos
Reply