Which PMIC part number is recommended for i.MX6 SoloX in temperature -40~105?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Which PMIC part number is recommended for i.MX6 SoloX in temperature -40~105?

跳至解决方案
2,133 次查看
m_c
Senior Contributor I

Which PMIC part number is recommended for i.MX6 SoloX in temperature -40~105?

标签 (1)
1 解答
1,997 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi,

You can use the MMPF0100F6ANES, first versions of the MCIMX6SX-SDB reference design used the MMPF0100 instead of the PF0200 (you can check the details in the schematic of the reference design) and the “F6” version is already pre-programmed to work with the IMX6 SoloX.

 

MMPF0100F6ANES is intended for use in extended industrial applications, so the operational temperature range for this part number goes from -40C to +105C.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,998 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi,

You can use the MMPF0100F6ANES, first versions of the MCIMX6SX-SDB reference design used the MMPF0100 instead of the PF0200 (you can check the details in the schematic of the reference design) and the “F6” version is already pre-programmed to work with the IMX6 SoloX.

 

MMPF0100F6ANES is intended for use in extended industrial applications, so the operational temperature range for this part number goes from -40C to +105C.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------