Using PF8200 in try-before-buy mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using PF8200 in try-before-buy mode

Jump to solution
2,387 Views
adevries
Contributor V

Hello,
In my current project I want to use the PF8200 in TBB/development mode initially. I want to use the programming interface on the KITPF8200FRDMPGM to program the PMIC, but I don't want the KITPF8200FRDMPGM to provide power to my board.

My plan is to prevent the KITPF8200FRDMPGM powering VDDIO by removing the jumper from J6, and prevent VIN being powered by removing the jumper from J8. I will then locally supply 5V to VIN and 3.3V to VDDIO. I have also been following the suggested programming interface found in figure 5 of AN12286 (see attached image).


Here are my questions:

1. If I power the PF8200 locally as I described, should I still be able to use the KITPF8200FRDMPGM programming interface?
2. From the datasheet, I see that VIN has certain rise time requirements (VIN must reach UVDET in 10 to 1500us). Does VDDIO have any similar requirements?
3. Does it matter whether VIN or VDDIO is applied first?

Thanks

Labels (2)
1 Solution
2,193 Views
jinyuzhang
NXP Employee
NXP Employee

1. If I power the PF8200 locally as I described, should I still be able to use the KITPF8200FRDMPGM programming interface?

Yes , I recommend you read the script which use to burn the OTP , the operation is so easy,  TBBEN is high ,PWRON is low , and then provide a 8V(you can even supply externally), then write the mirror register. TBBEN Low and VDDOTP low. 
2. From the datasheet, I see that VIN has certain rise time requirements (VIN must reach UVDET in 10 to 1500us). Does VDDIO have any similar requirements?

No,even for Vin ,there is also no requirement as you said, this is just tell customer the process for 5ms power up. so VDDIO and VIN ,just all keep on when you burn the OTP.
3. Does it matter whether VIN or VDDIO is applied first?

No,but i recommand VIn in front of VDDIO.

I upload a PPT in this link and you can also just use KL25Z to burn OTP on your board.

https://community.nxp.com/docs/DOC-344151 

PMIC and SBC question

View solution in original post

1 Reply
2,194 Views
jinyuzhang
NXP Employee
NXP Employee

1. If I power the PF8200 locally as I described, should I still be able to use the KITPF8200FRDMPGM programming interface?

Yes , I recommend you read the script which use to burn the OTP , the operation is so easy,  TBBEN is high ,PWRON is low , and then provide a 8V(you can even supply externally), then write the mirror register. TBBEN Low and VDDOTP low. 
2. From the datasheet, I see that VIN has certain rise time requirements (VIN must reach UVDET in 10 to 1500us). Does VDDIO have any similar requirements?

No,even for Vin ,there is also no requirement as you said, this is just tell customer the process for 5ms power up. so VDDIO and VIN ,just all keep on when you burn the OTP.
3. Does it matter whether VIN or VDDIO is applied first?

No,but i recommand VIn in front of VDDIO.

I upload a PPT in this link and you can also just use KL25Z to burn OTP on your board.

https://community.nxp.com/docs/DOC-344151 

PMIC and SBC question