UJA1132HW3V3 HVIO Read status issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UJA1132HW3V3 HVIO Read status issue

522 Views
13681887479
Contributor I

Hello,

I'm developing one product using UJA1132HW3V3 and S32K148. I'm trying to configure the HVIOs on UJA1132HW3V3 as wake up inputs and trying to read the status of the wake up input.

However, I got full zeros when using SBC_Transfer function in SDK to access the "Bank 0 wake-up status register" and "Bank 1 wake-up status register".

Meanwhile, I also could not read out the HVIOn(1-4, and 5-8) control registers using the SBC_Transfer function.

Can you support me on this topic? Thanks!

My SDK version is: S32SDK_S32K1xx_RTM_3.0.0

Tags (1)
0 Kudos
1 Reply

482 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello 13681887479@163.com,

Hard to say, it could be a HW issue.

Do you monitor the SPI bus with an oscilloscope?

Have you tried the sbc_uja113x_s32k148 SDK example?

Does it work?

Thanks,

BR, Daniel

0 Kudos