TJA1128 NO VCC output issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TJA1128 NO VCC output issues

5,923件の閲覧回数
Kavin_Kumaravel
Contributor II

Hello Team,

I am using TJA1128 in my control board, which is the primary source 5V for Micro. 

There is a failure with TJA, here are the info, could you let me know what could be the problem?

Note: LIN wake up is activated remote, I need to know why there is no 5V at VCC, and Reset is held LOW (may be under voltage at VCC)

PINMeasured Output in V
Wake17.93
Wake27.93
BAT13.36
LIN12.68
GND 
VCC0
  
TXD/SDI0
LIN_EN0
RST0
RXD0
WWD0
0 件の賞賛
返信
15 返答(返信)

5,789件の閲覧回数
Kavin_Kumaravel
Contributor II

Any ideas?

0 件の賞賛
返信

5,790件の閲覧回数
Kavin_Kumaravel
Contributor II

Any ideas on this? 

0 件の賞賛
返信

5,915件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Please share with the schematic!

0 件の賞賛
返信

5,908件の閲覧回数
Kavin_Kumaravel
Contributor II

Schematics

0 件の賞賛
返信

5,898件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Seems the SBC  triggers the OVERTEMP mode.

 

 

0 件の賞賛
返信

5,892件の閲覧回数
Kavin_Kumaravel
Contributor II
Currently, these data I have added is tested at 25 deg cel.
0 件の賞賛
返信

5,888件の閲覧回数
Kavin_Kumaravel
Contributor II
Measured voltage added to the initial question
0 件の賞賛
返信

5,890件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

which data you added?

 

0 件の賞賛
返信

5,913件の閲覧回数
Kavin_Kumaravel
Contributor II

Factor to consider,

TJA in my control board were working continuously for 78hrs at ambient temp of 65 deg, it failed at this point of time.

Interesting part is 4 samples failed between 70-90 hrs of continuous running at the same environment with the same issues.

0 件の賞賛
返信

5,886件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

So do you mean after power on SBC no VCC output? or after your high temperature test lost the VCC?

do you try to change new SBC test again?

 

0 件の賞賛
返信

5,882件の閲覧回数
Kavin_Kumaravel
Contributor II
When tested at high temp, over temp could trigger TJA to reset. Now I am testing at room temperature, But TJA is not recovered. Can you explain why is that case? Is this problem with register, incase of how do i do factory reset?
0 件の賞賛
返信

5,880件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Can you reproduce this issue with new SBC in your board?

 

0 件の賞賛
返信

5,876件の閲覧回数
Kavin_Kumaravel
Contributor II
No, at least not any time soon. Is it possible to do factory reset?
0 件の賞賛
返信

5,875件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

If so please read datasheet page18 -----6.3.4.2 Restoring factory preset values

0 件の賞賛
返信

5,873件の閲覧回数
Kavin_Kumaravel
Contributor II
I checked
All conditions passed, Vbat > Vth, LIN is held dominant and RSTN is low(0V) for more than 1 sec, but problem is RSTN is always LOW. I am assuming it means that SBC is not coming out of RESET loop?Any ideas why is that
0 件の賞賛
返信