TJA1128 NO VCC output issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1128 NO VCC output issues

5,630 Views
Kavin_Kumaravel
Contributor II

Hello Team,

I am using TJA1128 in my control board, which is the primary source 5V for Micro. 

There is a failure with TJA, here are the info, could you let me know what could be the problem?

Note: LIN wake up is activated remote, I need to know why there is no 5V at VCC, and Reset is held LOW (may be under voltage at VCC)

PINMeasured Output in V
Wake17.93
Wake27.93
BAT13.36
LIN12.68
GND 
VCC0
  
TXD/SDI0
LIN_EN0
RST0
RXD0
WWD0
0 Kudos
Reply
15 Replies

5,496 Views
Kavin_Kumaravel
Contributor II

Any ideas?

0 Kudos
Reply

5,497 Views
Kavin_Kumaravel
Contributor II

Any ideas on this? 

0 Kudos
Reply

5,622 Views
guoweisun
NXP TechSupport
NXP TechSupport

Please share with the schematic!

0 Kudos
Reply

5,615 Views
Kavin_Kumaravel
Contributor II

Schematics

0 Kudos
Reply

5,605 Views
guoweisun
NXP TechSupport
NXP TechSupport

Seems the SBC  triggers the OVERTEMP mode.

 

 

0 Kudos
Reply

5,599 Views
Kavin_Kumaravel
Contributor II
Currently, these data I have added is tested at 25 deg cel.
0 Kudos
Reply

5,595 Views
Kavin_Kumaravel
Contributor II
Measured voltage added to the initial question
0 Kudos
Reply

5,597 Views
guoweisun
NXP TechSupport
NXP TechSupport

which data you added?

 

0 Kudos
Reply

5,620 Views
Kavin_Kumaravel
Contributor II

Factor to consider,

TJA in my control board were working continuously for 78hrs at ambient temp of 65 deg, it failed at this point of time.

Interesting part is 4 samples failed between 70-90 hrs of continuous running at the same environment with the same issues.

0 Kudos
Reply

5,593 Views
guoweisun
NXP TechSupport
NXP TechSupport

So do you mean after power on SBC no VCC output? or after your high temperature test lost the VCC?

do you try to change new SBC test again?

 

0 Kudos
Reply

5,589 Views
Kavin_Kumaravel
Contributor II
When tested at high temp, over temp could trigger TJA to reset. Now I am testing at room temperature, But TJA is not recovered. Can you explain why is that case? Is this problem with register, incase of how do i do factory reset?
0 Kudos
Reply

5,587 Views
guoweisun
NXP TechSupport
NXP TechSupport

Can you reproduce this issue with new SBC in your board?

 

0 Kudos
Reply

5,583 Views
Kavin_Kumaravel
Contributor II
No, at least not any time soon. Is it possible to do factory reset?
0 Kudos
Reply

5,582 Views
guoweisun
NXP TechSupport
NXP TechSupport

If so please read datasheet page18 -----6.3.4.2 Restoring factory preset values

0 Kudos
Reply

5,580 Views
Kavin_Kumaravel
Contributor II
I checked
All conditions passed, Vbat > Vth, LIN is held dominant and RSTN is low(0V) for more than 1 sec, but problem is RSTN is always LOW. I am assuming it means that SBC is not coming out of RESET loop?Any ideas why is that
0 Kudos
Reply