transceiver
what is difference between TJA1029TK/20/1J versus TJA1029TK,118 ??
tx
The “,118”refers to the Packing, which for this case is Reel 13” Q1/T1.
“/1J” is used to identify this device as the dual source version of the device. We internally manufacture this device at two FAB locations in order to give our end customer built in dual sourcing for many of our devices. This code is used for the EDI ordering only so there is no technical reason behind.