TJA1029TK/20/1J

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1029TK/20/1J

1,150 Views
LKL77
Contributor I

transceiver

what is difference between TJA1029TK/20/1J versus TJA1029TK,118 ??

tx

0 Kudos
Reply
2 Replies

1,141 Views
reyes
NXP TechSupport
NXP TechSupport

The “,118”refers to the Packing, which for this case is Reel 13” Q1/T1. 

 “/1J” is used to identify this device as the dual source version of the device. We internally manufacture this device at two FAB locations in order to give our end customer built in dual sourcing for many of our devices. This code is used for the EDI ordering only so there is no technical reason behind.

0 Kudos
Reply

718 Views
Owen123
Contributor I

Hi NXP team :

Could you give the ePCN Note about the meaning of “/1J and ,118 ” for example, TJA1043/1J and TJA1043,118?

I search all the site but no Note about the question.

0 Kudos
Reply