Regarding the connection problem between the use of FS85 and Infineon MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding the connection problem between the use of FS85 and Infineon MCU

3,599 Views
sophie-wang
Contributor III
Dear NXP Expert,
According to the connection method between the SC33FS8510DNES and the TC397 in the , its RSTB pin is connected to the hardware reset of the MCU. However, in Figure 2 of the fs85 safety manual, the PGOOD is connected to the hardware reset, and the RSTB is connected to the software reset. I would like to ask whether the connection method between the SC33FS8510DNES and the TC397 in the NXP SBC Attach Aurix MCU can meet the safety requirements in the safety manual.
 
0 Kudos
Reply
5 Replies

3,585 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi Sophie

您能展示下客户的连接方式吗? RSTB是双向的,但是PGOOD只是输出而已

guoweisun_0-1739943468537.png

 

0 Kudos
Reply

3,580 Views
sophie-wang
Contributor III

Hi guowei,

感谢您的回复。客户的问题如下,我前面的附件里有相关的图

按照NXP SBC Attach Aurix MCU中SC33FS8510DNES与TC397的连接方式,它的RSTB引脚连接到MCU的硬件复位上,而在安全手册中Figure2上PGOOD连接到硬件复位,RSTB连接到软件复位。

请问如果按照NXP SBC Attach Aurix MCU中SC33FS8510DNES与TC397的连接方式是否满足安全手册中的安全需求?

BR

Sophie

0 Kudos
Reply

3,575 Views
guoweisun
NXP TechSupport
NXP TechSupport

那TC397的软复位pin连接到了哪里?

0 Kudos
Reply

3,567 Views
sophie-wang
Contributor III

Hi Guowei,

客户回复如下:

我提到的RSTB连接到软件复位,指的是根据SMUG中4.2.11的描述“FS85/FS84 RSTB pin is intended to be connected to the MCU Software Reset input (RSTB). When RSTB is asserted low, FS0B is also asserted low.”其中提到了RSTB连接到MCU的软件复位

我的理解:所谓的软件复位就是FS85的RSTB Pin拉低复位了MCU,不知道我理解的对吗?

Tags (1)
0 Kudos
Reply

3,551 Views
guoweisun
NXP TechSupport
NXP TechSupport

FS85的RSTB 可以复位MCU,当然MCU也可以通过控制pin去拉低RSTB从而去复位FS85,FS85 RSTB是双向的既可以输出也可以识别输入信号。

假如是RSTB接到了MCU的其他 可控制的pin他怎么能保证可控的去复位MCU 呢当FCCU发现MCU出现了问题需要做reset的时候?FCCU的错误不会触发PGOOD pin,但是会触发RSTB跟FS0B

 
 

 

 

PGOODpin也只是输出作用,并没有识别输入的功能。

看客户的应用吧,假如他这样设计自己能讲得通符合安全功能等级要求也是OK。

我们是推荐SBC的RSTB 直接连到MCU的RSTB or reset pin.

 

0 Kudos
Reply