I am trying to bring up a board using LS1046 and using a design similar to freeway board. I am using PF8100 and LTC7150 for multioutput voltages and VDD respectively. I am using programmable DC power supply for giving 3.3V,3 A and 12V,1.8A as input and not observing the expected voltages. Please find the attachment to see the measured and expected voltages. Please help me to resolve the problem.
Is there any software to simulate PF8100?
Thanks in advance
Thank you very much for your advice.
I will do as per your recommendations and let you know the outcome. Is there any software that we can simulate PF8100 and observe the waveforms? Is there any reason for the unexpected voltages?
Thanks in advance
No more the simulation model for this part.
Lots of reasons can lead to the error output,for example mistake on mount components/mistake for select regulator components/etcs.
Thank you very much for your prompt response. I am testing the power supply with the complete board, so that I hope each channel has load. Or please recommend me on adding load on each channel.
You can try to add external 500mA on such as 2.5V output channel, then test again.
Did you add the load on each channel? If not please add load to test again.