Please explain MC33665A Comparison Table

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Please explain MC33665A Comparison Table

跳至解决方案
1,145 次查看
rohans002
Contributor III

I have attached a comparison table mentioned on the product page of MC33665A where 2 IC are available.

I am not able to understand what exactly gateway means in this reference.
Does it mean that IC with CAN-FD gateway will communicate with MCU via CAN_FD and the same for SPI?

标记 (1)
0 项奖励
回复
1 解答
1,127 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Rohan,

there are two MC33665A versions. There used to be three versions, but MC33665A UART to TPL transceiver was withdrawn from production. There are left CAN FD to TPL transceiver (or gateway MC33665ATF4AE) and the SPI to TPL transceiver (or gateway ). Both of them are used for controlling of more, than one BCC (Battery Cell Controller e.g. MC33774A) with one MCU. Please refer to white paper which can be downloaded from the MC33774A product page

JozefKozon_0-1742380840176.png

In the prinscreen below the MC33665 is the SPI to TPL gateway.

JozefKozon_1-1742380889540.png

With Best Regards,

Jozef

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,128 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Rohan,

there are two MC33665A versions. There used to be three versions, but MC33665A UART to TPL transceiver was withdrawn from production. There are left CAN FD to TPL transceiver (or gateway MC33665ATF4AE) and the SPI to TPL transceiver (or gateway ). Both of them are used for controlling of more, than one BCC (Battery Cell Controller e.g. MC33774A) with one MCU. Please refer to white paper which can be downloaded from the MC33774A product page

JozefKozon_0-1742380840176.png

In the prinscreen below the MC33665 is the SPI to TPL gateway.

JozefKozon_1-1742380889540.png

With Best Regards,

Jozef

 

0 项奖励
回复
1,123 次查看
rohans002
Contributor III
thanks
0 项奖励
回复