Please explain MC33665A Comparison Table

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Please explain MC33665A Comparison Table

Jump to solution
1,285 Views
rohans002
Contributor III

I have attached a comparison table mentioned on the product page of MC33665A where 2 IC are available.

I am not able to understand what exactly gateway means in this reference.
Does it mean that IC with CAN-FD gateway will communicate with MCU via CAN_FD and the same for SPI?

Tags (1)
0 Kudos
Reply
1 Solution
1,267 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Rohan,

there are two MC33665A versions. There used to be three versions, but MC33665A UART to TPL transceiver was withdrawn from production. There are left CAN FD to TPL transceiver (or gateway MC33665ATF4AE) and the SPI to TPL transceiver (or gateway ). Both of them are used for controlling of more, than one BCC (Battery Cell Controller e.g. MC33774A) with one MCU. Please refer to white paper which can be downloaded from the MC33774A product page

JozefKozon_0-1742380840176.png

In the prinscreen below the MC33665 is the SPI to TPL gateway.

JozefKozon_1-1742380889540.png

With Best Regards,

Jozef

 

View solution in original post

0 Kudos
Reply
2 Replies
1,268 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Rohan,

there are two MC33665A versions. There used to be three versions, but MC33665A UART to TPL transceiver was withdrawn from production. There are left CAN FD to TPL transceiver (or gateway MC33665ATF4AE) and the SPI to TPL transceiver (or gateway ). Both of them are used for controlling of more, than one BCC (Battery Cell Controller e.g. MC33774A) with one MCU. Please refer to white paper which can be downloaded from the MC33774A product page

JozefKozon_0-1742380840176.png

In the prinscreen below the MC33665 is the SPI to TPL gateway.

JozefKozon_1-1742380889540.png

With Best Regards,

Jozef

 

0 Kudos
Reply
1,263 Views
rohans002
Contributor III
thanks
0 Kudos
Reply