PF8200 have officially acquired ASIL-B?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PF8200 have officially acquired ASIL-B?

1,000 Views
sangho92_kim
Contributor I

Hello,

I have a question about PF8200.

According to datasheet, PF8200 is complient with ASIL-B.

Is this means that PF8200 have officially acquired ASIL-B?

Labels (1)
1 Reply

888 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Sangho Kim,

PF8200 is ‘ASIL-B compliant’.

ASIL-B is a system level requirement, so, ASIL-B status cannot be granted to individual devices, however, PF8200 has official status to be in ASIL-B system (PF8200 meets all the requirements to be in an ASIL-B system).


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------