PF8200: VIN max rise time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PF8200: VIN max rise time

Jump to solution
1,140 Views
adevries
Contributor V

Hello,

In the PF8200 datasheet, Table 17 (image below) lists a minimum and maximum rise time for VIN to reach UVDET. Can an NXP employee explain the 1500us maximum rise time a bit more? If the VIN rise time is slower than that, will damage occur to the PMIC? If, in my application, I don't need to guarantee a 5 ms PMIC boot up time, is it acceptable for VIN to have a rise time slower than 1.5ms? Can VIN rise as slow as 100ms?

Thanks

adevries_0-1621365825743.png

 

Labels (3)
Tags (3)
0 Kudos
1 Solution
1,138 Views
guoweisun
NXP TechSupport
NXP TechSupport

No problem for VIN rise time above 1.5ms,this PF8200 will not damage.

View solution in original post

1 Reply
1,139 Views
guoweisun
NXP TechSupport
NXP TechSupport

No problem for VIN rise time above 1.5ms,this PF8200 will not damage.