Hello,
In the PF8200 datasheet, Table 17 (image below) lists a minimum and maximum rise time for VIN to reach UVDET. Can an NXP employee explain the 1500us maximum rise time a bit more? If the VIN rise time is slower than that, will damage occur to the PMIC? If, in my application, I don't need to guarantee a 5 ms PMIC boot up time, is it acceptable for VIN to have a rise time slower than 1.5ms? Can VIN rise as slow as 100ms?
Thanks
Solved! Go to Solution.
No problem for VIN rise time above 1.5ms,this PF8200 will not damage.
No problem for VIN rise time above 1.5ms,this PF8200 will not damage.