PF8100 VSNVS output Impossible Voltage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PF8100 VSNVS output Impossible Voltage

18,246 Views
chinachuli
Contributor II

when i modify "i.MX8QXP MEK schematic" to my own imx8qxp board, see attachment,i find VSNVS pin output at 5v, in datesheet VSNVS max output voltage is 3.3v. i do not know where is wrong, thanks for give me some suggesstion!

pastedImage_1.png

我在用官方IMX8QXP修改至自己的核心板,主要是简化了不必要的接口电路,原理图见附件,但我板子做回来测量发现VSNVS的输出有5V,而数据手册上最高电压为3.3V,找了很大时间未找出原因,所以求助论坛,非常感谢!

Labels (2)
Tags (1)
0 Kudos
Reply
8 Replies

17,850 Views
chinachuli
Contributor II

Simplify board to only have pmic part, schematic see attachment,VSNVS also output 5V, Where is wrong

0 Kudos
Reply

17,851 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

Do you connect with light load on this VSNVS output then see the actual output?

0 Kudos
Reply

17,850 Views
chinachuli
Contributor II

when VSNVS load 1k ,the actual output still is 5V 

0 Kudos
Reply

17,850 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Do you mind have a phone call with me?

Or give your phone number!

0 Kudos
Reply

17,851 Views
chinachuli
Contributor II

孙工:

我想用二层板做一块pf8100的测试板,原理图见附件。

在 2018-12-04 13:17:36,"褚立" <chinachuli@163.com> 写道:

HI:

我的电话:18158182825 褚立 非常感谢!

0 Kudos
Reply

17,851 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

可以这样做,或者你能预留一个Li-ion battery的位置方便调试,拉出来IIC的信号出来。

0 Kudos
Reply

17,850 Views
chinachuli
Contributor II

HI:

我的电话:18158182825 褚立 非常感谢!

0 Kudos
Reply

17,850 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

This should not PMIC's issue,you can disconnect VSNVS with your system only test VSNVS output to check PMIC good or not.

0 Kudos
Reply