Hi,
I am having some issue with a PF3001 powering an IMX6 solo. This problem is very rare but I would like to find the cause and fix it. Basically, sometime, the unit is not booting properly. I have read quite a bit of community question about the same problem but I haven't find a way to fix the issue I have.
It seem that the RTC_CLK on the IMX6 is not up fast enough sometime and this cause the unit not to boot. I looked at the POR_B on the PF3001 (or RESETBMCU) and it does go up a bit too fast. I looked into the data sheet to see if we could assert that pin directly but it doesn't seem so. I also try to use a delay with a RC on the PWRON but it was not enough (1M + 0.1µF on PWRON using VSNVS).
If someone could give a hint on where to look or how to delay the supplies, I would appreciate.
Thanks,
Fred