Hi,
We have a question regarding the PF1510. In the datasheet there is somethng unclear (for us at least).
- In order to properly work, does the PF1510 needs a VIN or can it be supplied by VSYS ?
- Is VSYS an input or an output ?
- If a Li-ion battery is connected to VSYS, it seems that LDO and SWx will not have a valid input when battery voltage has dropped around 3V1, is this correct ?
- Is this behaviour different on the PF1550 ?
- Do you have a typical application schematic for the PF1510 with a Li-ion battery supply ?
Regards
Thanks for the reply.
[gw]The VSYS voltage can be regulated to either 3.5 V, 3.7 V or 4.3 V
Does it mean that the input voltage of VSYS has to be regulated by an external IC (if VIN is not used)
- Is this behaviour different on the PF1550 ?
Could you develop a bit ? In my mind the PF1550 can be powered via an unregulated Li-ion battery, via which pin ?
- Is this behaviour different on the PF1550 ?
[gw] PF1550 page54- 8.6 Battery supplement mode, don’t have this function.
-Could you develop a bit ? In my mind the PF1550 can be powered via an unregulated Li-ion battery, via which pin ?
[gw]do you mean Battery supplement mode?
We have a question regarding the PF1510. In the datasheet there is something unclear (for us at least).
- In order to properly work, does the PF1510 needs a VIN or can it be supplied by VSYS ?
[gw]You can supplied it by VSYS or Vbus.
- Is VSYS an input or an output ?
[gw]VSYS is output of LDO and input of regulators.
- If a Li-ion battery is connected to VSYS, it seems that LDO and SWx will not have a valid input when battery voltage has dropped around 3V1, is this correct ?
[gw]The VSYS voltage can be regulated to either 3.5 V, 3.7 V or 4.3 V
- Is this behaviour different on the PF1550 ?
[gw]Yes.
- Do you have a typical application schematic for the PF1510 with a Li-ion battery supply ?
[gw]No