PF1510 EVK GUI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PF1510 EVK GUI

2,206 Views
russl
Contributor II

The PF1510_GUI_x64_Installer fails with error message that no JRE could be found. The requirements do not mention anything about needing a JRE. What version is needed? Will an Open JDK installation work? If so, what setup (reg keys etc. so installer can find the open JDK installation) is required for it to work? Or does this installer and resulting program need some JAVA browser plugin?

Labels (1)
0 Kudos
Reply
5 Replies

2,199 Views
russl
Contributor II

Thank you for the response guoweisun. I was hoping there was a way to use the JRE in OpenJDK. Can you comment on this matter at all?

0 Kudos
Reply

2,198 Views
guoweisun
NXP TechSupport
NXP TechSupport

For you side only install the Java JRE the GUI program will automatically call it when open this GUI.

0 Kudos
Reply

2,196 Views
russl
Contributor II

I understand I only need the JRE. But, as I have said twice now, I want to use the Open version, not the one referenced in the link you sent. Is this possible?

0 Kudos
Reply

2,191 Views
guoweisun
NXP TechSupport
NXP TechSupport

You can try to the open version but I usual download from the link and it works.

0 Kudos
Reply

2,201 Views
guoweisun
NXP TechSupport
NXP TechSupport

You can refer to below for Installing the Java JRE:

  1. Download Java JRE (Java SE Runtime Environment), available at http://

www.oracle.com/technetwork/java/javase/downloads/jre8-downloads-2133155.html

(8u162 or newer).

  1. Open the installer and follow the installation instructions.
  2. Following the successful installation, restart the computer.
0 Kudos
Reply