PF1510 EVK GUI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PF1510 EVK GUI

2,469 次查看
russl
Contributor II

The PF1510_GUI_x64_Installer fails with error message that no JRE could be found. The requirements do not mention anything about needing a JRE. What version is needed? Will an Open JDK installation work? If so, what setup (reg keys etc. so installer can find the open JDK installation) is required for it to work? Or does this installer and resulting program need some JAVA browser plugin?

标签 (1)
0 项奖励
回复
5 回复数

2,462 次查看
russl
Contributor II

Thank you for the response guoweisun. I was hoping there was a way to use the JRE in OpenJDK. Can you comment on this matter at all?

0 项奖励
回复

2,461 次查看
guoweisun
NXP TechSupport
NXP TechSupport

For you side only install the Java JRE the GUI program will automatically call it when open this GUI.

0 项奖励
回复

2,459 次查看
russl
Contributor II

I understand I only need the JRE. But, as I have said twice now, I want to use the Open version, not the one referenced in the link you sent. Is this possible?

0 项奖励
回复

2,454 次查看
guoweisun
NXP TechSupport
NXP TechSupport

You can try to the open version but I usual download from the link and it works.

0 项奖励
回复

2,464 次查看
guoweisun
NXP TechSupport
NXP TechSupport

You can refer to below for Installing the Java JRE:

  1. Download Java JRE (Java SE Runtime Environment), available at http://

www.oracle.com/technetwork/java/javase/downloads/jre8-downloads-2133155.html

(8u162 or newer).

  1. Open the installer and follow the installation instructions.
  2. Following the successful installation, restart the computer.
0 项奖励
回复