PCA9450 power dissipation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA9450 power dissipation

2,117 Views
Yakovs
Contributor I

Hello,

How to calculate the total Power Dissipation on the PCA9450 when powering the MIMX8ML8DVNLZAB? Is there typical PD or maybe you have a tool to calculate it?

Regards

0 Kudos
Reply
3 Replies

2,101 Views
Yakovs
Contributor I

Thank you,

I actually understand how to calculate the PD, but I'm at the very beginning of the design phase and need to estimate the calculated PD. So I was hoping you have a typical PCA9450 PD with a typical iMX8 power consumption. 

0 Kudos
Reply

2,083 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello, Sorry for the delay in replying, I have confirmed with the application team and we do not have a tool to calculate it. We apologize for the inconvenience this may cause you.

0 Kudos
Reply

2,106 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

PCA9450 integrates 6*DCCs and 5*LDOs, they work as one chip.

There are some methods to calculate the power Dissipation from each regulators to get the total power dissipation to get a ΔT with thermal resistors.
For DC-DC, Power Dissipation = Pinput * (1-efficiency);
For LDO, Power Dissipation = (Vin-Vout)*Iout;

then we can get the total power dissipation(P) of all the regulators, P*Rth(ja) = ΔT, Tambient + ΔT should be smaller than max Junction temperature (125℃)

ErikaC_0-1674250596568.pngErikaC_0-1674250596568.png

Hope it helps,

Regards.

0 Kudos
Reply