PCA9420 - "ON" push without effect

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCA9420 - "ON" push without effect

ソリューションへジャンプ
2,104件の閲覧回数
Gautier_Electronic
Contributor I

Hi community,

I would like to have fresh ideas about my current problem.

I use a PCA9420 on my design and I would like to use the feature which is doing an hard reset to the output rails when "ON" pin is turned '0' for a certain time.

I see that the "ON" is well turned '0', my PMIC is doing all goods output voltages but I can stay pressed for >16s no rails are going down. I have no idea about what could be bad in my design.

If anybody has an idea it will be well appreciated.

Regards

0 件の賞賛
返信
1 解決策
2,097件の閲覧回数
Gautier_Electronic
Contributor I

Hi community,

I found the solution. In my application it was necessary to disable SW1 which is not used. SW1 voltage output was not at the good value so SYSRSTn was pulled-down by the PCA9420. He looks like if the SYSRSTn is low the ON input algorithm is not working.

What was strange is, the ON mechanism didn't work but my LDO2/SW2 was enable and at my expected values.

Regards

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,098件の閲覧回数
Gautier_Electronic
Contributor I

Hi community,

I found the solution. In my application it was necessary to disable SW1 which is not used. SW1 voltage output was not at the good value so SYSRSTn was pulled-down by the PCA9420. He looks like if the SYSRSTn is low the ON input algorithm is not working.

What was strange is, the ON mechanism didn't work but my LDO2/SW2 was enable and at my expected values.

Regards

0 件の賞賛
返信