PCA9420 Charger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA9420 Charger

Jump to solution
1,294 Views
teruteru5678
Contributor I

I am developing a wearable device using the PC9420 and RT6 series.
It runs on a battery, so I need to charge it.

Question
1.After switching from MODE0 to standby with PWR_DN_EN=1, is it possible to charge it by inputting 5V to VIN?


2.After switching to standby with PWR_DN_EN=1, I would like to turn on the LED when charging is complete. Is this possible if I use the INT pin?
I would like the LED to light only when charging is complete.
Thank you in advance.

0 Kudos
Reply
1 Solution
1,220 Views
guoweisun
NXP TechSupport
NXP TechSupport
 
Hi Teruteru
Exactly we often recommend to use ship mode getting the charger active.
condition:
SHIP_EN=1 AND
VIN present AND
ON=1 AND
OPERATION_SEL_FROM_SHIPMODE=1
 
 
 
 
 
 
 
 

View solution in original post

0 Kudos
Reply
5 Replies
1,268 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi teruteru5678

Question
1.After switching from MODE0 to standby with PWR_DN_EN=1, is it possible to charge it by inputting 5V to VIN?

[gw]do you mean enable charger function under power down status?

 


Thanks!

 

BR

0 Kudos
Reply
1,259 Views
teruteru5678
Contributor I
Thank you for your reply.

Yes, that's right.

I would like to be able to charge the device even when it's turned off.

I understand that the device is turned off when it detects that it's ON and sets PWR_DN_EN=1,

but is this done incorrectly?
0 Kudos
Reply
1,251 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi 

I will test it next this function and give you feedback ASAP!

0 Kudos
Reply
1,226 Views
teruteru5678
Contributor I
Thank you.

I checked the data sheet and understood that it can be charged using ShipMode.

Do you generally use ShipMode to turn the power off (to save power)?

If so, I will use ShipMode.
0 Kudos
Reply
1,221 Views
guoweisun
NXP TechSupport
NXP TechSupport
 
Hi Teruteru
Exactly we often recommend to use ship mode getting the charger active.
condition:
SHIP_EN=1 AND
VIN present AND
ON=1 AND
OPERATION_SEL_FROM_SHIPMODE=1
 
 
 
 
 
 
 
 
0 Kudos
Reply