Need to satisfy the requirement of cell balancing of 1A using AFE MC33771C

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need to satisfy the requirement of cell balancing of 1A using AFE MC33771C

2,334件の閲覧回数
Vishal_Pandey
Contributor II

Hi, 

We have encountered situation where We require 1A in cell balancing, currently our setup  supports till 300mA(AFE's max capability). Can you suggest us solutions to satisfy our 1A cell balancing requirement. Can you also look into the diagram in the file attached to this message and verify whether this is possible ?. Differential max voltage across the MOSFET which is 10V is also not breached. 

Thanks in Advance,

Vishal

 

 

Cell Balancing @ 1A.png

ラベル(1)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

2,322件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Vishal,

The device supports external MOSFETs for passive balancing in order to increase the max balancing current.

There is an example schematic and safety analysis available for that, but they are confidential requiring an NDA in place. I would recommend you to create a standard support ticket to sign the NDA if needed and then ask for both the schematic as well as safety analysis.

Best regards,

Tomas

0 件の賞賛
返信

2,330件の閲覧回数
Vishal_Pandey
Contributor II

I feel even the diagram that I have attached in previous message  wont work due to internal Op-amp's config(shown in below image) which might throw fault.

AFE internal cell balancing structure.png

0 件の賞賛
返信

973件の閲覧回数
divyam
Contributor II

Hi @Vishal_Pandey 

Any success in getting the reference design/schematic for external cell balancing?

0 件の賞賛
返信