Maximum force for applying heatsink

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Maximum force for applying heatsink

跳至解决方案
489 次查看
jeroenvanandel
Contributor I

What is the maximum force for the following components:

PMIC:  PCA9450CHNY & PCA9450AAHNY:  56 HVQFN  package

0 项奖励
回复
1 解答
470 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

We do not specify a maximum heatsink mounting force. We recommend to use thermal vias and a large ground pad under the EP to spread heat to the PCB. This is the primary intended method for thermal dissipation. If in your application a heatsink must be mounted on top, JEDEC recommends ≤20N for small QFN packages.

BRs, Tomas

在原帖中查看解决方案

1 回复
471 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

We do not specify a maximum heatsink mounting force. We recommend to use thermal vias and a large ground pad under the EP to spread heat to the PCB. This is the primary intended method for thermal dissipation. If in your application a heatsink must be mounted on top, JEDEC recommends ≤20N for small QFN packages.

BRs, Tomas