MW7IC2020NT1 impedance matching

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MW7IC2020NT1 impedance matching

637 Views
Ari3l
Contributor I

Hi, I need to match MW7IC2020NT1 PA output impedance.  I would like to know:

1) According to the list on the Datasheet Figure 11, should I assume that the impedance looking towards the output signal pin is the reflected value of Zload?

2) How does Power supply value affect the listed values ? (i.e. using Vdd = 14 V instead of 28 V)

 

Tags (1)
0 Kudos
Reply
1 Reply

614 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

Thank you for contacting us.

1. Yes, please see our process to measure the Zin and Zload in this application note AN1107 page 7.

2. Please note that our reference designs are stated for a specified set of operating conditions, PO, VCC and frequency. If you want to change any condition you have to adapt your circuit.

Hope this helps.

0 Kudos
Reply