MC34PF3001A7EP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC34PF3001A7EP

1,317件の閲覧回数
shwethanarayan
Contributor I

Hi,

 

Please find the attachment. We are using IMX6 Ultralite processor for one of our project. We have a small query in PMIC PF3001.

 

1. What is the SW1_SEQ, SW2_SEQ and so on?

2. If it is a sequence, then why in A7 series it is mentioned as 3 everywhere.for SW1_SEQ, SW2_SEQ and so on.

3. Do you have EVK with PMIC PF3001 for IMX6 Ultralite?

Please let me know the answers for the above queries.

 

Regards

ShwethaCapture.JPG

0 件の賞賛
返信
1 返信

1,311件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi,

[A1] The SW1_SEQ, SW2_SEQ and so on depends on the OTP configuration, for example, for the A7 (the one you highlighted), all the enabled regulators starts at sequence ‘3’, but the V33 regulator which starts at sequence ‘2’.

 

[A2] The SEQ_CLK_SPEED is set to 2.0ms, which means that every regulator set to SEQ ‘3’, will turn-on after 3 times SEQ_CLK_SPEED (2.0ms), so, 6ms after power-on the device. Same with the regulators set to SEQ ‘2’, these will turn-on 4ms after power-on the device.

 

[A3] Unfortunately no, the is no EVK with PMIC PF3001 for IMX6 Ultralite, there is a reference design, however, it is not publicly available, you need to request it with your NXP Authorized Distributor by signing an NDA.

 

Regards,

Jose

0 件の賞賛
返信