MC33771 SPI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC33771 SPI

1,625 次查看
mohamed-moustafa
Contributor I

How can i know SPI commands to control PGA or IC at all ?

0 项奖励
回复
2 回复数

1,613 次查看
mohamed-moustafa
Contributor I

I cannot access those files 
where I have no response on my NDA request.

What should I do?

 

0 项奖励
回复

1,615 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Mohamed,

The setting of the PGA gain in manual or automatic mode can be performed by configuring ADC_CFG[PGA_GAIN] register (0x06).

ADC_CFG.JPG

The setting of the PGA gain in automatic mode will also be performed by the automatic gain control. Automatic gain control allows the device to obtain the most appropriate gain setting for the amplifier input signal level. In automatic gain control mode, the conversion result is digitally compared with internally programmed thresholds.

Figure 14.JPG

You might find useful information about programming/setting the MC33771 in the AN12084 (MC3371/MC33772 Programming Guide) which is available on the product website under Secure Files requiring an NDA:

AN.JPG

In the Software section under Secure Files is also available complete BCC Software Driver:

Driver.JPG

Best regards,

Tomas

0 项奖励
回复