MC33730 linear regulators

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC33730 linear regulators

1,458 次查看
alessandrocorti
Contributor II

Hello all,

I'm going to use the MC3370 chip in an environment where I need only the 5V and the 3.3V voltages.

I don't need to use any stand by supplies, I know the VKAM is always active (also with the chip in sleep mode) and this is ok for me, I want to use VDDL as 3.3V source and I don't need more.

To save power in stand by, I want to program the VDD3 regulator as 3.3V, not stand by regulator, but I don't need it because I use the VDDL regulator as 3.3V source, here my question, have I to add the external pass NPN transistor and bypass capacitors to the VDD3 circuitry (VDD3_B and VDD3), or can I simply left open these two pins (VDD3_B and VDD3)?

Thanks a lot,

Regards.

Alessandro

0 项奖励
回复
2 回复数

1,396 次查看
alessandrocorti
Contributor II

Thank you G.w. Sun,

so there isn't at all the risk to damage the linear regulator or may be the entire chip?, I mean, the stage that should drive the external pass transistor (may be an op amp?) works always in saturation because of the absence of the feedback voltage, I think..

Regards,

Alessandro

0 项奖励
回复

1,396 次查看
guoweisun
NXP TechSupport
NXP TechSupport

HI Alessandro

After discussed ,to be on safe consider please add the external pass NPN transistor and bypass capacitors to the VDD3 circuitry (VDD3_B and VDD3) if unused this LDO

0 项奖励
回复