Issue with MC34VR5100A1EP chip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue with MC34VR5100A1EP chip

Jump to solution
2,555 Views
minalnemade
Contributor II

Hi,

       We have build custom board with LS1012A and PMIC chip MC34VR5100A1EP. We are facing issue of VSNVS output from PMIC chip. We are providing 3.3V input to PMIC chip but we are not getting VSNVS output inspite of Vin voltage > 3.1V. We have connected VSNVS output to EN pin of PMIC chip. As VSNVS output is missing PMIC chip is not getting enabled and hence it is not generating any output voltages. As per data-sheet of PMIC chip VSNVS output can not be disabled and is generated after Vin voltage > 3.1V (UVDET). Inspite of this condition being met we observed that VSNVS output is not generated by PMIC chip. We are not using coin cell battery input and hence LICELL input of PMIC chip is bypassed to ground through 0.1uf capacitor. All connections of PMIC chip are as per the reference design of LS1012AFRDM. Please let's know what could be the issue.

 

regards

Minal

0 Kudos
1 Solution
2,348 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

Can you double check your VSNVS connection in your system except VSNVS connect with EN?

It seems that VSNVS has current limit.

View solution in original post

0 Kudos
7 Replies
2,348 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

Please note the output current of VSNVS(1mA) and you'd better give us your schematic.

0 Kudos
2,348 Views
minalnemade
Contributor II

Hi Jive,

Please find attached schematics.

Regards

Minal

0 Kudos
2,348 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

Disconnect VSNVS and EN,you can use external signal to control EN then to check this issue.

0 Kudos
2,348 Views
minalnemade
Contributor II

Hi Jive,

We have directly connected 3.3V through 4.7K resistor but we observed

that output voltages randomly comes up and then goes back down.

Please guide.

Thanks & Regards

Minal

0 Kudos
2,348 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

Do you mean that disconnect with EN and VSNVS then supply EN with external 3.3V with 4.7K resistor?

Do you monitor the VSNVS value when you do above operation?

0 Kudos
2,348 Views
minalnemade
Contributor II

Hi,

yes .. we have disconnected EN and VSNVS then supply EN with external

3.3V with 4.7K resistor.

We observed VSNVS to be randomly increasing and going down. It goes max to

2.3V

Thanks & Regards

Minal

0 Kudos
2,349 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

Can you double check your VSNVS connection in your system except VSNVS connect with EN?

It seems that VSNVS has current limit.

0 Kudos