Identify MC33771C or MC33772C over SPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Identify MC33771C or MC33772C over SPI

Jump to solution
542 Views
tbondar
Contributor II

I'm writing firmware for a hardware design where either the 7 cell or the 14 cell version of the chip can be populated. I would like to handle both in the same firmware. Is there a way to ask the BCC chip to tell me which version it is? I've glossed through the datasheet but didn't find a register that would return a device ID or something similar. Thanks!

Tags (2)
0 Kudos
Reply
1 Solution
527 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Tamás,

You are right, neither the MC33771C nor the MC33772C includes a dedicated identification register like WHO_AM_I. This means there is no simple or direct way to identify the BCC over SPI. Anyway, I guess you may try reading from a register that only exists or is valid on one of the BCCs. For example, read MEAS_CELL7 or higher. If the read returns valid data, the device is an MC33771C.

BRs, Tomas

View solution in original post

0 Kudos
Reply
1 Reply
528 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Tamás,

You are right, neither the MC33771C nor the MC33772C includes a dedicated identification register like WHO_AM_I. This means there is no simple or direct way to identify the BCC over SPI. Anyway, I guess you may try reading from a register that only exists or is valid on one of the BCCs. For example, read MEAS_CELL7 or higher. If the read returns valid data, the device is an MC33771C.

BRs, Tomas

0 Kudos
Reply