How to download program in normal mode(not in debud mode)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to download program in normal mode(not in debud mode)?

7,640件の閲覧回数
dingsg
Contributor I

hi !

     I have a question about FS65xx  when I download  program.when I use  FS65xx to supply  power MCU in normal mode(not in debug mode),if i want to downloade a new program  by using  bootloader ,what should  i do?    And now I use IO port to pull up DEBUG pin in bootloader ,and release it in APP when download process is finished. Because I don't want to feed dog in download process.  How should  I operate FS65 in bootloader and it will meet functional safety  requirments.

Thanks!

ラベル(1)
0 件の賞賛
返信
14 返答(返信)

7,494件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

What kind of MCU platform do you select in your system?

0 件の賞賛
返信

7,089件の閲覧回数
xupei
Contributor I

Hello,

After reading it, I still don't understand the title question。

How to download program in normal mode(not in debud mode,e.g thru CAN )?thanks

"The watchdog refresh can be disabled during INIT_FS state of the fail-safe logic to allow programming without taking care of the watchdog refresh. INIT_FS can be entered by a reset request with RSTB_REQ bit in SF_OUTPUT_REQUEST register."The above is described in the guideline.

0 件の賞賛
返信

7,494件の閲覧回数
dingsg
Contributor I

Hi !

There are two kinds of MCU Platform,  they are MPC5775E and Infineon Aurix TC38x.

When using the two platforms, is there any difference in the function usage of fs65 ?

Thanks!

0 件の賞賛
返信

7,494件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

This is MCU MPC5775 related questions,I send your driver code based on MPC5774 platform, hope could help you!

0 件の賞賛
返信

7,494件の閲覧回数
dingsg
Contributor I

Thank you for your reply!

            I have a question ,Could you tell me if we need to feed watchdog when  we download the program? if needn't ,how should we deal with the Debug pin?

0 件の賞賛
返信

7,494件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Download program in debug mode,no need to feed watchdog.

0 件の賞賛
返信

7,494件の閲覧回数
dingsg
Contributor I

  When fault occurs  ,  it can only be cleared by watchdog refresh ?

0 件の賞賛
返信

7,493件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

你说的什么种类的错误?

0 件の賞賛
返信

7,494件の閲覧回数
dingsg
Contributor I

过压故障产生后故障错误计数器会增加,这时候应该怎么清除故障呢

0 件の賞賛
返信

7,494件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

你的电话是多少?

0 件の賞賛
返信

7,494件の閲覧回数
dingsg
Contributor I

你好!我们在第一次烧写程序的时候,这时候即不能通过MCU去控制debug引脚,也不能实现正常喂狗,应该如何做操呢?

0 件の賞賛
返信

7,494件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

这样只能自己做外围的电路,上电默认满足进入debug模式

0 件の賞賛
返信

7,494件の閲覧回数
dingsg
Contributor I

座机电话:021-34978900 转 8740

手机号码:15821852057

0 件の賞賛
返信

7,494件の閲覧回数
dingsg
Contributor I

When we download program ,we use IO port to pullup Debug pin and release the pin in application  after download process has been finished, Does this approach meet functional safety requirements?

0 件の賞賛
返信