How to clear SBC FS4500 DIAG_VSUP_VCAN->ILIM_CAN & DIAG_SPI->SPI_REQ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to clear SBC FS4500 DIAG_VSUP_VCAN->ILIM_CAN & DIAG_SPI->SPI_REQ?

1,642 次查看
juliusjai
Contributor II

I'm working on DIAG monitor for SBC FS4500 and I have encountered DIAG_VSUP_VCAN->ILIM_CAN and

DIAG_SPI->SPI_REQ are always set. In fact CAN communication is working well and the SBC output power supply is very stable.

Does anybody has idea to avoid this behavior?

Thanks,

Julius

标签 (1)
0 项奖励
回复
2 回复数

1,438 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi,

ILIM_CAN and SPI_REQ are cleared when reading these bits or with a Power On reset.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,438 次查看
phanendravarma_
Contributor II

Hello Jose, 

I had similar problem.

I operated chip in Debug mode to analyze spi commands.

But while reading the MODE register it always giving chip is in Normal Mode(instead of INIT mode) . and whenreading HWCONFIG debug bit it's responding with debug mode is not enabled. 

One more observation was SPI_REQ bit in Diag register was always Set never cleared after Read or POR. 

Any inputs from your side were highly appreciated .

Thanks

PVR

0 项奖励
回复