How to bypass the impact of VCORE_FB_UV, VAUX_UV and VCCA_UV when using SBC4500

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to bypass the impact of VCORE_FB_UV, VAUX_UV and VCCA_UV when using SBC4500

1,213 Views
xinguang_wang
Contributor III

Hi,

when I using FS4500CAE chip to manage S32K144 power fault, I encountered some questions as below.

  1. This has three errors which is VCORE_FB_UV, VAUX_UV and VCCA_UV. Due to these errors, the RSTB and FS0B  pins are low, ABIST1 is not OK as well. And I can't enter INIT_FS mode to bypass the impact of them.
  2. When I enter Debug mode(Of course, there are errors above), and main state machine is normal mode, the register states about CAN has no error, but I can't get message from can box using laptop. My same program works OK on another board which has the same MCU pin about CAN, I wonder to know why it doesn't work.

I'm very appreciated if you could give me any suggestions about it.

Thanks a lot!

Xinguang

Labels (1)
Tags (2)
0 Kudos
4 Replies

1,071 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Please provide your schematic of SBC ?

0 Kudos

1,071 Views
xinguang_wang
Contributor III

Hi G.w.

my schematic of SBC is as below:

pastedImage_1.png

Is there any problem?

Thanks a lot and Best Regards!

Xinguang

0 Kudos

1,071 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

I attached the schematic for your reference,please also tell your phone number!

0 Kudos

1,071 Views
xinguang_wang
Contributor III

Hi G.w.

Thanks you very much, my phone number is 17737597085.

Best Regards!

Xinguang

0 Kudos