So I followed the step by step instructions on powering up the PMIC KITPF0100EPEVBE board. I connected the PF programmer (KITPFPGMEVME) to the board via the 8-conductor flat ribbon cable and the USB to my computer (FYI, I tried this for my windows 7 and 10 machines). The USB was detected and the driver installed. I then proceeded to install the KITPFGUI software. The software installed correctly and the log showed that the device was found.
I tried clicking on the other tabs but they wouldn't open. when I clicked on "Scan For Devices" button I would get the error "Object reference not set to an instance of an object." And I would click ok about 6 times for the error to clear.
I then proceeded to click on the Enable Target checkbox and I got the error "No Target Detected!"
Here is a picture of my hardware connected via the PF-programmer
and I also connected it directly via the mini USB port. I was able to read some voltages.
Please, any assistance will be greatly appreciated. For now, this is a show stopper for me. Thanks.
Solved! Go to Solution.
Hi Kerry,
Seems like you are missing the VIN 3.6V power supply connection.
Thanks for your explicit answer.
Thank you.