How do I get my KITPF0100EPEVBE board connected to my KITPFGUI 4.0 graphical user interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I get my KITPF0100EPEVBE board connected to my KITPFGUI 4.0 graphical user interface

Jump to solution
2,056 Views
raven123crow
Contributor II

So I followed the step by step instructions on powering up the PMIC KITPF0100EPEVBE board. I connected the PF programmer (KITPFPGMEVME)  to the board via the 8-conductor flat ribbon cable and the USB to my computer (FYI, I tried this for my windows 7 and 10 machines). The USB was detected and the driver installed. I then proceeded to install the KITPFGUI software. The software installed correctly and the log showed that the device was found.2018-11-27_19-56-47.png

I tried clicking on the other tabs but they wouldn't open. when I clicked on "Scan For Devices" button I would get the error "Object reference not set to an instance of an object." And I would click ok about 6 times for the error to clear.

2018-11-27_19-57-48.png

I then proceeded to click on the Enable Target checkbox and I got the error "No Target Detected!"

2018-11-27_19-57-24.png

Here is a picture of my hardware connected via the PF-programmer

IMG_20181127_195908.jpg

and I also connected it directly via the mini USB port. I was able to read some voltages.

IMG_20181127_201932.jpg

Please, any assistance will be greatly appreciated. For now, this is a show stopper for me. Thanks.

Labels (2)
1 Solution
1,854 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

Please read attached page6 for hardware connection setting.

View solution in original post

4 Replies
1,854 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Kerry,

Seems like you are missing the VIN 3.6V power supply connection.

1,854 Views
raven123crow
Contributor II

Thanks for your explicit answer. 

0 Kudos
1,855 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

Please read attached page6 for hardware connection setting.

1,854 Views
raven123crow
Contributor II

Thank you.

0 Kudos