FS8530: Is OTP Programming/Burning possible for variants other than A0 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FS8530: Is OTP Programming/Burning possible for variants other than A0 ?

ソリューションへジャンプ
1,983件の閲覧回数
BL_
Contributor III

Hello NXP experts,

we're having the FS8530A1 samples and want to perform a OTP programming using FlexGUI.

By emulation everything works well, however by OTP programming an error occurred with the message "WP flag is present"

Since this information is for us currently very urgent, we hope to hear from you soon.

Thanks very much.

BL

ラベル(1)
タグ(2)
0 件の賞賛
1 解決策
1,980件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

A1 version means had already done OTP and can't be done again!

元の投稿で解決策を見る

0 件の賞賛
3 返答(返信)
1,977件の閲覧回数
BL_
Contributor III

Hi,

thanks. It is clear now why we couldn't perform a OTP programming via FlexGUI for A1 version.

 

Thanks,

BL

0 件の賞賛
1,981件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

A1 version means had already done OTP and can't be done again!

0 件の賞賛
890件の閲覧回数
sezensonmez
Contributor II
Is there any way to disable write protection? UM11183 says "The device configuration can be changed three times". I didn't see any expression that the A1 version can not be programmed 2nd or 3rd times. It just expressed as pre-programmed. So, regrettably, we bought a lot of A1 version and now we have to send back this SBCs.
0 件の賞賛