FS84

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决
4,603 次查看
liubenjun
Contributor I

Hi NXP team,

    For FS84,Can I read Main OTP_REGISTERS data?If it can be read, please tell me how.Thanks!

标签 (1)
0 项奖励
回复
1 解答
4,516 次查看
guoweisun
NXP TechSupport
NXP TechSupport

这些regulators输出的值都是您选择的或者自己预定的,AMUX读出来的值您比较下就知道了,但是OTP寄存器里面的数值一般不再客户端支持读取。

在原帖中查看解决方案

0 项奖励
回复
8 回复数
4,517 次查看
guoweisun
NXP TechSupport
NXP TechSupport

这些regulators输出的值都是您选择的或者自己预定的,AMUX读出来的值您比较下就知道了,但是OTP寄存器里面的数值一般不再客户端支持读取。

0 项奖励
回复
4,503 次查看
liubenjun
Contributor I

谢谢!我知道预设的电压值了。

0 项奖励
回复
4,512 次查看
liubenjun
Contributor I

这些regulators输出的值是硬件还是软件设定的?

0 项奖励
回复
4,535 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Do you know the value you set about these regulators?

0 项奖励
回复
4,520 次查看
liubenjun
Contributor I

 

Isn't the regulator configured by OTP?Are these voltages related to the Main OTP_REGISTERS configuration?

 

微信截图_20201106102157.png微信截图_20201106102243.png

0 项奖励
回复
4,588 次查看
guoweisun
NXP TechSupport
NXP TechSupport

hi

Unfortunately I am afraid that you can't read it out!

0 项奖励
回复
4,546 次查看
liubenjun
Contributor I

Okay,Thank you for your reply,I have another question,I read some voltage values from the M_AMUX register as follows: VDDIO voltage = 3.23V, VBUCK1 voltage = 1.25V, VBUCK3 voltage = 2.32V, VPRE voltage = 3.29V, VBOOST voltage = 5.78V, etc. How do I know these voltage values are correct.

0 项奖励
回复
4,529 次查看
liubenjun
Contributor I

Thanks, and I read some voltage values ​​through M_AMUX register. For example: VDDIO voltage = 3.23V, VBUCK1 voltage = 1.25V, VBOOST voltage = 5.78V.So, how do I know that these voltage values ​​are correct.

0 项奖励
回复
An error has occurred when reading existing sub-variable "Language_PG_Configuration"; see cause exception! The type of the containing value was: extended_hash+string (lithium.coreapi.webui.template.models.NamedValueByNameTemplateModel wrapped into f.e.b.StringModel) ---- FTL stack trace ("~" means nesting-related): - Failed at: #assign redirect_lingo_page_url = web... [in template "language_macro_header.ftl" at line 173, column 1] - Reached through: #include "language_macro_header.ftl" [in template "Language_translator_Dashboard" at line 3, column 1] ----