FS6500 CAN Communication

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FS6500 CAN Communication

3,493 次查看
mmurugesh
Contributor II

Hi,

I am using FS6500. I just want to use it as CAN transceiver. I don't want to implement any safety related features.

Should I need to configure or check any registers in FS6500 through SPI?

If any, pls give your advice.

标签 (1)
0 项奖励
回复
5 回复数

2,966 次查看
AllanAn
NXP Employee
NXP Employee

Hi Murugesh,

some registers of FS6500  can only be configured in the initial phase; some can be configured in normal mode;

register.PNG

please see the picture below about the SPI:

SPI.PNG

  SPI2.PNG

for more details, please refer to the datasheet of FS4500~FS6500 in the https://www.nxp.com/webapp/sps/download/mod_download.jsp?colCode=FS6500-FS4500&appType=moderatedWith...

Brs

Allan

0 项奖励
回复

2,966 次查看
AllanAn
NXP Employee
NXP Employee

Hi Murugesh ,

    Thank you for the question,

    First, CAN_5V voltage regulator is not a safety regulator:

can1.PNG

    Secondly, when you use FS1b, you should refer to INIT_FAULT register to configure FS1B_CAN_IMPACT to 0, which will be configured in the initial phase.

can2.PNG

for more detailed, please refer to https://www.nxp.com/webapp/sps/download/mod_download.jsp?colCode=FS6500-FS4500&appType=moderatedWith...

Help this will help you

Best regards

Allan An

0 项奖励
回复

2,966 次查看
mmurugesh
Contributor II

Hi Allan,

Thanks for the reply.

I would like to just elaborate my question..

Previously i was working with NXP evaluation board and used FlexCAN0 in MPC5744P. The CAN transceiver used in that board was MC33901. It's a standalone CAN transceiver. CAN communication was working good enough.

Now instead of MC33901, i used FS6500 and made the CAN interface connections as depicted in the application note. But the CAN communication is not working.

My question is... Should i need to configure any of the registers in the FS6500 through SPI before starting the CAN communication?

I just only want to have CAN communication. I am not interested in any of the safety related features right now.

0 项奖励
回复

2,966 次查看
AllanAn
NXP Employee
NXP Employee

Hi Murugesh,

    OK, got it , you should configure CAN_LIN_MODE register, configure CAN_MODE_1:0 to "11",

the default CAN state is sleep;

can3.PNG

    if the problem is still exist please check DIAG_VSUP_VCAN and DIAG_CAN_FD registers to find if there are CAN power supply and physical connection errors.

   Help this will help you.

  Brs

  Allan An

0 项奖励
回复

2,966 次查看
mmurugesh
Contributor II

I am trying to write the FS6500 registers. But it is unsuccessful.

I want to know about the SPI wave format to be used..

1. Classical SPI or Modified SPI transfer format?

2. About the Clock polarity and phases?

0 项奖励
回复