FS6500 CAN BUS off

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,128件の閲覧回数
witness
Contributor III

hi, experts Now I am working on a project based on S32k324&FS6500, as for FS6500, we use it as SBC and CAN transceiver. but for CAN bus off testing, only CANH->GND can cause bus off, CANH->CANL and CANL->VCC won't cause CAN bus off. besides, another CAN node of S32K324 which use TJA1043 as tranceiver, the three cases can be able to cause CAN bus off, so I suspect may some FS6500 register have not been set properly, anyone can give me a clue? thanks. 

0 件の賞賛
返信
1 解決策
3,084件の閲覧回数
witness
Contributor III

Issue fixed, the reason is related to hardware design, there is a limit current resistor near the CANH and CANL of SBC, just remove it.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,110件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Ming,

Please see below about FS6500 capability to detect CANH/CANL shorts to BATT/GND.

Capture.JPG

BR, Tomas

0 件の賞賛
返信
3,100件の閲覧回数
witness
Contributor III

hi, Tomas

Thanks for your reply, I have noticed the information you have mentioned, but currently, except CANH -> GND, for another two case(CANL->VCC, CANH->CANL), SBC CAN TX and RX electrical level keep same, so it seems like the chip can not detect the failure.

0 件の賞賛
返信
3,085件の閲覧回数
witness
Contributor III

Issue fixed, the reason is related to hardware design, there is a limit current resistor near the CANH and CANL of SBC, just remove it.

0 件の賞賛
返信