FS26 unable to enter DFS State on KITFS26SKTEVM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FS26 unable to enter DFS State on KITFS26SKTEVM

1,198 次查看
RChatterjee
Contributor III

On programming FS26 using KITFS26SKTEVM Rev E, it is programmed in emulation mode with the following configuration (using FS26 GUI FS26):

1. Wake1 Event triggers DFS Exit

2. DFS Enable is set to when FS0B or RSTB is asserted.

In this mode, when RSTB is held low, even after more than 30s, the FS26 is not entering DFS mode.

Can such a functionality be tested when running in emulation?

PFA images of said configuration

标签 (1)
0 项奖励
回复
1 回复

1,150 次查看
guoweisun
NXP TechSupport
NXP TechSupport

 

Had replied based on case 00621526

 

0 项奖励
回复